Finding the Right Jobsite Lights Could Save You Thousands

Having the right Jobsite lights during a construction project is not only a matter of increased productivity—it can mean the difference between a safe work area and an unsafe one.

That’s why the Occupational Safety and Health Administration (OSHA) has a minimum standards code for the requirements of lighting for construction areas to ensure that workers are able to remain safe while performing their jobs.

While OSHA uses the term “foot candles,” that term is outdated, as it refers to the amount of light one candle would give to an area covering one square foot. Today’s lighting is measured by lumen or lux, and you can think of one foot candle as being one lumen per square foot. It’s important to note that the OSHA standards don’t apply to industrial sites, such as warehouses and shipyards, as these locations must meet the American National Standard A11. 1-2965, R1970.

Batteries vs. Cords

There are several different types of lights available as Jobsite lights that offer extensive benefits over older styles that have been used in the past. And while the average business spends $5,120 a year in corded lights with extension cords, they could save up to $5,000 over the course of five years by investing in newer, high-powered cordless lights.

With the convenient, cordless Jobsite lights available on the market today, you can even buy one light that can illuminate 9,000 lumens at a 360-degree radius and is stackable. These types of lights are excellent ways to illuminate large spaces and come with USB lithium batteries for a full 14 hours of operation before needing to be recharged.

LED Lights Have Changed the Industry

The best advancement to Jobsite lights has been LED. In the past, due to the cheaply made nature of CFL lighting, contractors often considered lights to be disposable after the job is complete, increasing their costs by having to buy a new set when the next job starts. In contrast, LED lights not only last longer, they save energy with an 80 percent lower consumption rate. They also offer sustainability for five years or more—and that includes running them around the clock. 

Not Going Dark

Another important aspect of battery-powered, LED lighting is that it allows a contractor to keep a worksite illuminated over weekends and nights when work is not being done. Having a dark Jobsite is not only uninviting to future tenants (because it makes the building look abandoned and scary), it also invites the homeless and criminals to enter the site after hours.

The average business spends $1,900 a year on three-day shutdowns. That’s $9,500 over the course of five years. However, purchasing a compact LED cordless light like this one can save $8,578 over five years—that’s enough to buy a two-year lease on a Ford F-150 work truck!

For more information on how to save money on your Jobsite lights, contact the Jobsite lighting experts at Milwaukee. We’re here to help you save money and keep your workers safe and productive.