Sump, Sewage & Effluent Pumps & Accessories - Motion Industries

Sump, Sewage & Effluent Pumps & Accessories

Submersible Pumps are centrifugal pumps where the motor and liquid end of the pump are submerged in the liquid being pumped. They can pump clean liquids(sump), slightly dirty liquids (effluent), or solids (sewage) materials. The impeller design and flow, as well as port size, generally determine the application of these types of pumps. The motor and voltage is specific to the impeller and application, as a general rule. Solids handling, or sewage pumps, are able to pump clean water, but generally not as efficiently as impellers designed specifically for clean water; solids handling or sewage pumps have larger openings in the impeller to pass solids. However, the clean water pumps will clog if used in an application where the sewage pump is required. Submersible pumps are used in applications where the pump can be kept below the grade in a pit, minimizing floor space for the pumps as well as discharging the liquid below grade if needed.

Results for “Sump, Sewage & Effluent Pumps & Accessories”
Narrow Your Search

Frequently Purchased Sump, Sewage & Effluent Pumps & Accessories